This catalog figures the Modicon M41 range of plcs: from presentation, trough description, communication I/O compatibility, options, and references.
Ghidul utilizatorului
Modicon M241 Logic Controller, Hardware Guide
English
2022-07-15
Modicon M241 Logic Controller, Hardware Guide
Use this document to:
- Install and operate your M241 Logic Controller.
- Connect the M241 Logic Controller to a programming device equipped with EcoStruxure Machine Expert software.
- Interface the M241 Logic Controller with I/O expansion modules, HMI, and other devices.
- Familiarize yourself with the M241 Logic Controller features.
Modicon M241 Logic Controller, User Guide
English
2022-07-15
Firmware
Last Release Notes
English
2022-07-15
M241 M251 Firmware
English
2022-07-15
M241 M251 Firmware
This new firmware corrects several bugs, there is no functionality integrated. Details available in Release Notes.
The firmware is delivered in 2 different shapes, for SD card or Seco package for SoMachine v4.3. According to your preferred way to update the firmware, you can select one shape or another.
M241 M251 Firmware
English
2022-07-15
M241 M251 Firmware
This new firmware correct an issue identified by the Err LED blinking and the PLC not booting.
The firmware is delivered in 2 different shapes, for SD card or Seco package for SoMachine v4.3. According to your preferred way to update the firmware, you can select one shape or another.
New firmware for M241 v4.0.6.41
English
2022-07-15
New firmware for M241 v4.0.6.41
This new firmware updates the memory driver to integrate new component references, and corrects several anomalies, with details in the Release Notes.
New firmware for M241 v4.0.6.42
English
2022-07-15
New firmware for M241 v4.0.6.42
This new firmware address the anomaly of M241 firmware update with V5.0.8.4, with LED Error blinking.
MSX Configurator is obsolete, it’s replaced by Modicon PLC Configurator. This new web based tool provides more functionalities and ergonomic. Selecting the right PLC and IOs has never been so easy and fast. Save time during design and implementation into your project. To access Modicon PLC Configurator, follow the link: https://www.se.com/ww/en/work/products/industrial-automation-control/tools/modicon-plc-configurator.jsp
UL Certificate Ordinary Location TM241 TM251 TMC4 TM3X
SILENT
2022-07-15
Ghid de utilizare sistem
Compact Hardwired Logic Controller M241, System User Guide
English
2022-07-15
Compact Hardwired Logic Controller M241, System User Guide
This document describes a generic architecture based on Modicon M241 Logic Controller and is intended to provide a quick introduction to the described system.