This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
Tanúsítvány
DoC
Russian
2024-05-15
Környezetvédelmi közzététel
PEP-Metallic Mounting plate
English
2024-05-15
Brosúra
Műanyag és üvegszál erősítésű poliészter szekrények brosúra
Hungarian
2024-05-15
Megfelelőségi nyilatkozat
NSYSFP400 EU RoHS nyilatkozat
Hungarian
2024-05-25
NSYSFP400 EU RoHS nyilatkozat
Rögzítőkészlet villanypóznához
NSYSFP400 Kínai RoHS nyilatkozat
Hungarian
2024-05-25
NSYSFP400 Kínai RoHS nyilatkozat
Rögzítőkészlet villanypóznához
NSYSFP400 REACh nyilatkozat
Hungarian
2024-05-25
NSYSFP400 REACh nyilatkozat
Rögzítőkészlet villanypóznához
Használati útmutató adatlap
Thalassa PLM General Instruction for post fixing device
SILENT
2024-05-15
CAD
Thalassa PLM - Post fastening for PLM54/64 - 3D CAD