Link Positions (Factory Mounted) Diagram for 2 to 5-step Stepping Switches Select the number of steps according to the product characteristics.
Marking
Angular Position of Switch
Switching Program
Convention Used for Switching Program Representation
Contact closed
Contact closed in 2 positions and maintained between the 2 positions
Sealed assembly for auto-maintain control
Overlapping contacts
Spring return position: for a switching angle of 90°, spring return is over 30° after the last position (for a maximum of 3 simultaneous contacts). Example:
|