Schneider-Electric
 
K1C003ALH picture- web-product-data-sheet
K1C003ALH
Harmony K1, K2, Cam switch, 3 poles , 45°, 12 A, screw mounting
Schneider Electric
Technical Description
Link Positions (Factory Mounted)
Diagram for 1 to 6-pole Switches

Select the number of poles according to the product characteristics.


I1
Input 1
I2
Input 2
O1
Output 1
O2
Output 2


Marking



Angular Position of Switch



Switching Program
Diagram for 1 to 6-pole Switches

Select the number of poles according to the product characteristics.


(1)
1-pole
(2)
2-pole
(3)
3-pole
(4)
4-pole
(5)
5-pole
(6)
6-pole


Convention Used for Switching Program Representation

Contact closed

Contact closed in 2 positions and maintained between the 2 positions

Sealed assembly for auto-maintain control

Overlapping contacts

Spring return position: for a switching angle of 90°, spring return is over 30° after the last position (for a maximum of 3 simultaneous contacts).

Example: