Schneider-Electric
 
ZB4BP5 картинка- Schneider-electric
ZB4BP5
Глава за несветещ бутон, Harmony XB4, метал, издаден, жълт, 22 мм, пружинно връщане, с предпазно капаче, без маркировка
Schneider Electric
Technical Description
Electrical Composition Corresponding to Code C1



Electrical Composition Corresponding to Code C2



Electrical Composition Corresponding to Codes C9, C11, SF1 and SR1



Electrical Composition Corresponding to Code C15

1 N/O


1 N/C


1 N/O + N/C or 1 N/O + N/O or 1 N/C + N/C



Legend

Single contact


Double contact


Light block


Possible location