Schneider-Electric
 
XB5FA3341C0 slika – Schneider-electric
XB5FA3341C0
Push button, Harmony XB5, flush mounted, plastic, white, 30mm, spring return, marked with black up arrow, 1 NO, grey color plated bezel
Schneider Electric
Technical Description
Electrical Composition Corresponding to Code C1



Electrical Composition Corresponding to Code C2



Electrical Composition Corresponding to Codes C9, C11, SF1 and SR1



Electrical Composition Corresponding to Code C15

1 N/O


1 N/C


1 N/O + N/C or 1 N/O + N/O or 1 N/C + N/C



Legend

Single contact


Double contact


Light block


Possible location