Function L : Asymmetrical Flasher Relay (Starting Pulse Off) Description Repetitive cycle comprises of two, independently adjustable timing periods Ta and Tr. Each timing period corresponds to a different state of the output R. Function: 1 Output
Function Li : Asymmetrical Flasher Relay (Starting Pulse On) Description Repetitive cycle comprises of two, independently adjustable timing periods Ta and Tr. Each timing period corresponds to a different state of the output R. Function: 1 Output
Legend
Relay de-energised
Relay energised
Output open
Output closed C | Control contact | G | Gate | R | Relay or solid state output | R1/R2 | 2 timed outputs | R2 inst. | The second output is instantaneous if the right position is selected | T | Timing period | Ta - | Adjustable On-delay | Tr - | Adjustable Off-delay | U | Supply |
|