Schneider-Electric
 
K1H004PL slika – Schneider-electric
K1H004PL
Ohišje za 2-stopenjsko motorno stikalo - 3 poli - 60° - 12 A - vijačna montaža
Schneider Electric
Technical Description
Link Positions (Factory Mounted)



Angular Position of Switch



Switching Program



Convention Used for Switching Program Representation

Contact closed

Contact closed in 2 positions and maintained between the 2 positions

Sealed assembly for auto-maintain control

Overlapping contacts

Spring return position: for a switching angle of 90°, spring return is over 30° after the last position (for a maximum of 3 simultaneous contacts).

Example: