Schneider-Electric
 
K10H014UCH picture- Schneider-electric
K10H014UCH
Harmony K komplett bütykös kapcsoló, 10A, Ø16-22mm furat, 4P, 60°, 2 fokozatú átkapcsoló
Schneider Electric
Technical Description
Link Positions (Factory Mounted)
Diagram for 1 to 4-pole Switches

Select the number of poles according to the product characteristics.



Marking



Angular Position of Switch



Switching Program
Diagram for 1 to 4-pole Switches

Select the number of poles according to the product characteristics.


(1)
1-pole
(2)
2-pole
(3)
3-pole
(4)
4-pole


Convention Used for Switching Program Representation

Contact closed

Contact closed in 2 positions and maintained between the 2 positions

Sealed assembly for auto-maintain control

Overlapping contacts

Spring return position: for a switching angle of 90°, spring return is over 30° after the last position (for a maximum of 3 simultaneous contacts).

Example: