Schneider-Electric
 
K1F003MCH
K1F003MCH
Comutator Ampermetric Cu Came - 3 Circuite - 90° - 12 A - Pentru Ø 22 Mm
Schneider Electric
Technical Description
Link Positions (Factory Mounted)



Marking



Angular Position of Switch



Switching Program



Convention Used for Switching Program Representation

Contact closed

Contact closed in 2 positions and maintained between the 2 positions

Sealed assembly for auto-maintain control

Overlapping contacts

Spring return position: for a switching angle of 90°, spring return is over 30° after the last position (for a maximum of 3 simultaneous contacts).

Example: