Link Positions (Factory Mounted) Diagram for 1 to 4-pole Switches Select the number of poles according to the product characteristics
Marking
Angular Position of Switch
Switching Program
Convention Used for Switching Program Representation
Contact closed
Contact closed in 2 positions and maintained between the 2 positions
Sealed assembly for auto-maintain control
Overlapping contacts
Spring return position: for a switching angle of 90°, spring return is over 30° after the last position (for a maximum of 3 simultaneous contacts). Example:
|