Schneider-Electric Riverbank Electrical Wholesalers Ltd
 
ATS22D47Q picture- riverbankelectrical
ATS22D47Q
soft starter-ATS22-control 220V-power 230V(11kW)/400...440V(22kW)
Local distributor code Local distributor code: 
393439087
EAN Code EAN Code: 
3606480167201
Schneider Electric
Mounting and Clearance
Precautions
Standards

The Altistart 22 soft starter is compliant with pollution Degree 2 as defined in NEMA ICS1-1 or IEC 60664-1.

For environment pollution degree 3, install the Altistart 22 soft starter inside a cabinet type 12 or IP54.

DANGER

HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH

ATS22 soft starters are open devices and must be mounted in a suitable enclosure.

Failure to follow these instructions will result in death or serious injury.

Air Circulation

Leave sufficient free space to help the air required for cooling purposes to circulate from the bottom to the top of the unit.


Overheating

To avoid the soft starter to overheat, respect the following recommendations:

  • Mount the Altistart 22 Soft Starter within ± 10° of vertical.

  • Do not locate the Altistart 22 Soft Starter near heat radiating elements.

  • Electrical current through the Altistart 22 Soft Starter will result in heat losses that must be dissipated into the ambient air immediately surrounding the soft starter. To help prevent a thermal fault, provide sufficient enclosure cooling and/or ventilation to limit the ambient temperature around the soft starter.

  • If several soft starters are installed in a control panel, arrange them in a row. Do not stack soft starters. Heat generated from the bottom soft starter can adversely affect the ambient temperature around the top soft starter.


Mounting
Connection Between the Fan and the Altistart 22 Soft Starter


1
Altistart 22 Soft Starter
2
Fan


Wall mounted or Floor-standing Enclosure with IP 23 Degree of protection
Introduction

To help proper air circulation in the soft starter, grilles and forced ventilation can be installed.

Ventilation Grilles


Forced Ventilation Unit