Antenna Mounting
The antenna is installed following his vertical axis
Antenna Clearance in a Metal Enclosure
The range is reduced if the transmitter is placed in a metal enclosure (reduction factor:approx 10%). Glass window | 10...20 % | Plaster wall | 30...45 % | Brick wall | 60 % | Concrete wall | 70...80 % | Metal structure | 50...100 % |
|