Mounting Recommendations
Depending on the conditions in which the drive is to be used, its installation will require certain precautions and the use of appropriate accessories. Install the unit vertically: Clearance
Mounting Types Type A Mounting
Type B Mounting
Type C Mounting
By removing the protective blanking cover from the top of the drive, the degree of protection for the drive becomes IP 20. The protective blanking cover may vary according to the drive model (refer to the user guide). The protective blanking cover must be removed from ATV 71P•••N4Z drives when they are mounted in a dust and damp proof enclosure.
Specific Recommendations for Mounting the Drive in an Enclosure Ventilation To ensure proper air circulation in the drive:
Dust and Damp Proof Metal Enclosure (IP 54) The drive must be mounted in a dust and damp proof enclosure in certain environmental conditions: dust, corrosive gases, high humidity with risk of condensation and dripping water, splashing liquid, etc. This enables the drive to be used in an enclosure where the maximum internal temperature reaches 50°C.
|