Depending on the conditions in which the drive is to be used, its installation will require certain precautions and the use of appropriate accessories.
Install the unit vertically:
Do not place it close to heating elements.
Leave sufficient free space to ensure that the air required for cooling purposes can circulate from bottom to the top of the unit.