|
|
|
ATV950D30N4
variable speed drive, ATV950, 30kW, 400/480V, with braking unit, IP55
|
|
|
Clearances
X1 | X2 | X3 |
---|
≥ 100 mm (3.94 in.) | ≥ 100 mm (3.94 in.) | ≥ 10 mm (0.39 in.) |
Mount the device in a vertical position (±10°). This is required for cooling the device. Do not mount the device close to heat sources. Leave sufficient free space so that the air required for cooling purposes can circulate from the bottom to the top of the drive.
|
|