Thermal-Magnetic Tripping Curves for GV4P, GV4PE, GV4PEM Average Operating Times at 20 °C Related to Multiples of the Setting Current Hot state
Cold state
Current Limitation on Short-Circuit for GV4P, GV4PE, GV4PEM (3-Phase 400/415 V) Dynamic Stress I peak = f (prospective Isc) at 1.05 Ue = 435 V
Thermal Limit on Short-Circuit for GV4P, GV4PE, GV4PEM Thermal Limit in kA22s in the Magnetic Operating Zone Sum of I2dt = f (prospective Isc) at 1.05 Ue = 435 V
|