Schneider-Electric JS System
 
ATV320U40M3C picture- jssystems
ATV320U40M3C
변속 드라이브, Altivar Machine ATV320, 4 kW, 200...240 V, 3상, 컴팩트
Schneider Electric
Connections and Schema
Connection Diagrams
Diagram with Line Contactor

Connection diagrams conforming to standards ISO13849 category 1 and IEC/EN 61508 capacity SIL1, stopping category 0 in accordance with standard IEC/EN 60204-1.


(1)
Line choke (if used)
(2)
Fault relay contacts, for remote signaling of drive status

Diagram with Switch Disconnect

Connection diagrams conforming to standards EN 954-1 category 1 and IEC/EN 61508 capacity SIL1, stopping category 0 in accordance with standard IEC/EN 60204-1.


(1)
Line choke (if used)
(2)
Fault relay contacts, for remote signaling of drive status


Control Connection Diagram in Source Mode


(1)
Analog output
(2)
Analog inputs
(3)
Reference potentiometer (10 kOhm maxi)
(4)
Digital inputs


Digital Inputs Wiring

The logic input switch (SW1) is used to adapt the operation of the logic inputs to the technology of the programmable controller outputs.

Switch SW1 set to “Source” position and use of the output power supply for the DIs.


Switch SW1 set to “Source” position and use of an external power supply for the DIs.


Switch SW1 set to “Sink Int” position and use of the output power supply for the DIs.


Switch SW1 set to “Sink Ext” position and use of an external power supply for the DIs.