Digital Inputs Wiring Diagram
(1) : The COM0, COM1 and COM2 terminals are not connected internally (A) : Sink wiring (positive logic) (B) : Source wiring (negative logic) Fast Input Wiring (I0...I7)
Fast Transistor Outputs Wiring Diagram
Transistor Outputs Wiring Diagram
(1) : The V1+, V2+ and V3+ terminals are not connected internally. (2) : The V1–, V2– and V3– terminals are not connected internally.
USB Mini-B Connection
Ethernet Connection to a PC
|