Inapoi
Descoperiti TM241C24T de la
Caracteristici
Dimensions Drawings
Mounting and Clearance
Connections and Schema
Descarcare si documente
Discover your Schneider-Electric tools
TM241C24T
Automat Programabil M241 24 Io Tranzistor Pnp
Descarcare TM241C24T fise de date
Model CAD 3D
Connections and Schema
Digital Inputs
Wiring Diagram
(*) :
Type T fuse
(1) :
The COM0, COM1 and COM2 terminals are not connected internally
(A) :
Sink wiring (positive logic)
(B) :
Source wiring (negative logic)
Fast Input Wiring (I0...I7)
Fast Transistor Outputs
Wiring Diagram
(*) :
2 A fast-blow fuse
Transistor Outputs
Wiring Diagram
(*) :
Type T fuse
(1) :
The V1+ and V2+ terminals are not connected internally.
(2) :
The V1– and V2– terminals are not connected internally.
USB Mini-B Connection