Schneider-Electric Riverbank Electrical Wholesalers Ltd
 
ATV212HU15N4 picture- riverbankelectrical
ATV212HU15N4
variable speed drive ATV212 - 1.5kW - 2hp - 480V - 3ph - EMC - IP21
Schneider Electric
Connections and Schema
Recommended Wiring Diagram
3-Phase Power Supply


A1:
ATV 212 drive
KM1:
Contactor
Q1:
Circuit breaker
Q2:
GV2 L rated at twice the nominal primary current of T1
Q3:
GB2CB05
S1, S2:
XB4 B or XB5 A pushbuttons
T1:
100 VA transformer 220 V secondary
(1)
Fault relay contacts for remote signalling of the drive status
(2)
Connection of the common for the logic inputs depends on the positioning of the switch (Source, PLC, Sink)
(3)
Reference potentiometer SZ1RV1202

NOTE: All terminals are located at the bottom of the drive. Install interference suppressors on all inductive circuits near the drive or connected on the same circuit, such as relays, contactors, solenoid valves, fluorescent lighting, etc.

Switches (Factory Settings)

Voltage/current selection for analog I/O (VIA and VIB)


Voltage/current selection for analog I/O (FM)


Selection of logic type


(1)
negative logic
(2)
positive logic


Other Possible Wiring Diagrams
Logic Inputs According to the Position of the Logic Type Switch

“Source” position


“Sink” position


“PLC” position with PLC transistor outputs


(1)
PLC


(1)
PLC

2-wire control


F:
Forward
R:
Preset speed
(2)
ATV 212 control terminals

3-wire control


F:
Forward
R:
Stop
RES:
Reverse
(2)
ATV 212 control terminals

PTC probe


(2)
ATV 212 control terminals
(3)
Motor

Analog Inputs

Voltage analog inputs

External +10 V


(2)
ATV 212 control terminals
(4)
Speed reference potentiometer 2.2 to 10 kΩ


(2)
ATV 212 control terminals

Analog input configured for current: 0-20 mA, 4-20 mA, X-Y mA


(2)
ATV 212 control terminals
(5)
Source 0-20 mA, 4-20 mA, X-Y mA

Analog input VIA configured as positive logic input (“Source” position)


(2)
ATV 212 control terminals

Analog input VIA configured as negative logic input (“Sink” position)


(2)
ATV 212 control terminals