Schneider-Electric Riverbank Electrical Wholesalers Ltd
 
XACB085 picture- riverbankelectrical
XACB085
empty pendant control station XAC-B - 8 vertical openings
Schneider Electric
Connections and Schema
Control of Single-Speed Reversing Motor

With XESD1181 contact block, to be ordered separately



Control of 2-Speed Reversing Motor

With XESD1281 contact block, to be ordered separately


KM
High speed contactor


Control of Single-Speed Reversing Motor 2-Phase Switching

With XESD1191 contact block, to be ordered separately


Combined with 3-pole isolating block XACS399 or XACS3991, shown in the unoperated position (pendant station “supplied”), fitted with key release trigger action latching Emergency stop operator.



Control of 2-Speed Reversing Motor 2-Phase Switching

With XESD1291 contact block, to be ordered separately



Control of Single-Speed Reversing Motor 3-Phase switching, Reversing by 2-Phase Inversion

With XESD2201 contact block, to be ordered separately



Control of Single-Speed Reversing Motor 3-Phase switching, Reversing by 2-Phase Inversion

With XESD2241 contact block, to be ordered separately