|
|
|
TM3DM24RG
Discrete I/O module, Modicon TM3, 24 IO (16 inputs, 8 relay outputs, spring) 24 VDC
|
|
|
Digital Mixed I/O Module (24-channel) Wiring Diagram (Source)
(1) The COM0, COM1 and COM2 terminals are not connected internally. (2) To improve the life time of the contacts, and to protect from potential inductive load damage, it is recommended to connect a free wheeling diode in parallel to each inductive DC load or an RC snubber in parallel of each inductive AC load. (A) Sink wiring (positive logic) (C) Source wiring (positive logic) Wiring Diagram (Sink)
(1) The COM0, COM1 and COM2 terminals are not connected internally. (2) To improve the life time of the contacts, and to protect from potential inductive load damage, it is recommended to connect a free wheeling diode in parallel to each inductive DC load or an RC snubber in parallel of each inductive AC load. (B) Source wiring (negative logic) (D) Sink wiring (negative logic)
|
|