Schneider-Electric
 
TM3DQ8R picture- web-product-data-sheet
TM3DQ8R
Discrete output module, Modicon TM3, 8 relay outputs (screw) 24 VDC
Schneider Electric
Connections and Schema
Digital Relay Output Module (8-channel)
Wiring Diagram (Positive Logic)


(*)
Type T Fuse
(1)
The COM0 and COM1 terminals are not connected internally.
(2)
To improve the life time of the contacts, and to protect from potential inductive load damage, it is recommended to connect a free wheeling diode in parallel to each inductive DC load or an RC snubber in parallel of each inductive AC load.
(A)
Source wiring (positive logic)

Wiring Diagram (Negative Logic)


(*)
Type T fuse
(1)
The COM0 and COM1 terminals are not connected internally.
(2)
To improve the life time of the contacts, and to protect from potential inductive load damage, it is recommended to connect a free wheeling diode in parallel to each inductive DC load or an RC snubber in parallel of each inductive AC load.
(B)
Sink wiring (negative logic)