Recommended Wiring Diagram 3-Phase Power Supply
Q2: GV2 L rated at twice the nominal primary current of T1 S1, S2: XB4 B or XB5 A pushbuttons T1: 100 VA transformer 220 V secondary (1) Fault relay contacts for remote signalling of the drive status (2) Connection of the common for the logic inputs depends on the positioning of the switch (Source, PLC, Sink) (3) Reference potentiometer SZ1RV1202 NOTE: All terminals are located at the bottom of the drive. Install interference suppressors on all inductive circuits near the drive or connected on the same circuit, such as relays, contactors, solenoid valves, fluorescent lighting, etc. Switches (Factory Settings) Voltage/current selection for analog I/O (VIA and VIB)
Voltage/current selection for analog I/O (FM)
Selection of logic type
Other Possible Wiring Diagrams Logic Inputs According to the Position of the Logic Type Switch “Source” position
“Sink” position
“PLC” position with PLC transistor outputs |
|
|
2-wire control
(2) ATV 212 control terminals 3-wire control
(2) ATV 212 control terminals PTC probe
(2) ATV 212 control terminals Analog Inputs Voltage analog inputs External +10 V |
(2) ATV 212 control terminals (4) Speed reference potentiometer 2.2 to 10 kΩ |
(2) ATV 212 control terminals |
Analog input configured for current: 0-20 mA, 4-20 mA, X-Y mA
(2) ATV 212 control terminals (5) Source 0-20 mA, 4-20 mA, X-Y mA Analog input VIA configured as positive logic input (“Source” position)
(2) ATV 212 control terminals Analog input VIA configured as negative logic input (“Sink” position)
(2) ATV 212 control terminals
|