Connections Connector Wiring
(2) : External setting pushbutton or XXZPB100 remote teach pushbutton. Pin number | Wire color | Description |
---|
1 | BN: Brown | +12…24VDC | 2 | WH: White | Input teach | 3 | BU: Blue | 0 VDC | 4 | BK: Black | Output | 5 | GY: Grey | Synchronization |
Wiring Scheme. Digital Output (NO or NC)
Wiring for the Synchronization Function (Side by Side Application)
NOTE: Up to 8 sensors can be synchronized to operate side by side by electrically connecting all pin no.5 (grey) wires together. To synchronize more than 8 sensors, a PLC output can be used (the pins no.5 must be simultaneously driven by the rising edge of a pulse).
|