Schneider-Electric
 
TM241CE40T picture- Schneider-electric
TM241CE40T
controller M241 40 IO transistor PNP Ethernet
EAN Code EAN Code: 
3606480611209
Schneider Electric
Connections and Schema
Digital Inputs
Wiring Diagram


(*) :
Type T fuse
(1) :
The COM0, COM1 and COM2 terminals are not connected internally
(A) :
Sink wiring (positive logic)
(B) :
Source wiring (negative logic)

Fast Input Wiring (I0...I7)



Fast Transistor Outputs
Wiring Diagram


(*) :
2 A fast-blow fuse


Transistor Outputs
Wiring Diagram


(*) :
Type T fuse
(1) :
The V1+, V2+ and V3+ terminals are not connected internally.
(2) :
The V1–, V2– and V3– terminals are not connected internally.


USB Mini-B Connection



Ethernet Connection to a PC