This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Conformiteitsverklaring
AK2CD100 China RoHS-verklaring
Dutch
2024-06-17
AK2CD100 China RoHS-verklaring
Deksel voor kabelgoot - PVC - Grijs - 100x2000mm - Set van 8
AK2CD100 EU RoHS-verklaring
Dutch
2024-06-17
AK2CD100 EU RoHS-verklaring
Deksel voor kabelgoot - PVC - Grijs - 100x2000mm - Set van 8
AK2CD100 REACh-verklaring
Dutch
2024-06-17
AK2CD100 REACh-verklaring
Deksel voor kabelgoot - PVC - Grijs - 100x2000mm - Set van 8