This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Declaração de Conformidade
04651 Declaração RoHS da China
Portuguese
2024-04-01
04651 Declaração RoHS da China
LINERGY LGY LATERAL BUSBAR SUPPORT
04651 Declaração RoHS da UE
Portuguese
2024-04-01
04651 Declaração RoHS da UE
LINERGY LGY LATERAL BUSBAR SUPPORT
Folha de instruções
Linergy LGY - Busbar supports - Lateral profiles up to 3200 A