This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
In exposed environments, particular attention must be paid to the choice of enclosures. Stainless steel is the solution to resist aggression in exposed environments. This guide will help the reader to select the optimum stainless-steel enclosure accordingly.
Environmental disclosure
SPACIAL S3X - Stainless Steel
English
2024-04-15
CAE
Spacial S3X CAE package for EPLAN
SILENT
2024-04-15
Declaration of conformity
NSYPFCX China RoHS Declaration
English
2024-04-02
NSYPFCX China RoHS Declaration
4 wall fixing brackets in stainless steel AISI 304 for Spacial S3X
NSYPFCX EU RoHS Declaration
English
2024-04-02
NSYPFCX EU RoHS Declaration
4 wall fixing brackets in stainless steel AISI 304 for Spacial S3X
NSYPFCX REACh Declaration
English
2024-04-02
NSYPFCX REACh Declaration
4 wall fixing brackets in stainless steel AISI 304 for Spacial S3X
Instruction sheet
IS - CRN - Wall-fixing lugs
SILENT
2024-04-15
CAD
CAD Drawing - 3D STP Format -Set of 4 304L stainless-steel wall fixing lugs for Spacial S3X