This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Certificat
C-FR.AJ40.B.01205_20
Russian
2024-04-15
Declaratie de conformitate
NSYBTE630TBT Declaratie RoHS China
Romanian
2024-03-25
NSYBTE630TBT Declaratie RoHS China
Terminale De Jonctiune Cu Trei Poli. Sectiune Cablu Jonctiune (Mm²) 35 La 120.
NSYBTE630TBT Declaratie RoHS UE
Romanian
2024-03-25
NSYBTE630TBT Declaratie RoHS UE
Terminale De Jonctiune Cu Trei Poli. Sectiune Cablu Jonctiune (Mm²) 35 La 120.