This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
In exposed environments, particular attention must be paid to the choice of enclosures. Stainless steel is the solution to resist aggression in exposed environments. This guide will help the reader to select the optimum stainless-steel enclosure accordingly.
Declaratie de mediu
SPACIAL S3X - Stainless Steel
English
2024-04-15
CAE
Spacial S3X CAE package for EPLAN
SILENT
2024-04-15
Declaratie de conformitate
NSYPFC2X Declaratie REACh
Romanian
2024-03-29
NSYPFC2X Declaratie REACh
4 Console De Fixare In Perete Din Otel Inoxidabil Aisi 316L Prntru Spacial S3X
NSYPFC2X Declaratie RoHS China
Romanian
2024-03-29
NSYPFC2X Declaratie RoHS China
4 Console De Fixare In Perete Din Otel Inoxidabil Aisi 316L Prntru Spacial S3X
NSYPFC2X Declaratie RoHS UE
Romanian
2024-03-29
NSYPFC2X Declaratie RoHS UE
4 Console De Fixare In Perete Din Otel Inoxidabil Aisi 316L Prntru Spacial S3X
Fişa de instrucţiuni
IS - CRN - Wall-fixing lugs
SILENT
2024-04-15
CAD
CAD Drawing - 3D STP Format -Set of 4 316L stainless-steel wall fixing lugs for Spacial S3X