This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Certificat
DoC
Russian
2024-04-15
UL_CoC_Spacial_SF-SFHD-SFP-SFM-SFE-SF6G
English
2024-04-15
ЕАЭС_N_RU_Д-FR.PA01.B.80899_20
Russian
2024-04-15
Declaratie de mediu
UE_Spacial SF, Steel floor-standing enclosure
English
2024-04-15
Declaratie de conformitate
NSYSF12680E Declaratie REACh
Romanian
2024-04-24
NSYSF12680E Declaratie REACh
Spacial Sf Carcasa Electronica - Asamblata - 1200X600X800 Mm
NSYSF12680E Declaratie RoHS China
Romanian
2024-04-24
NSYSF12680E Declaratie RoHS China
Spacial Sf Carcasa Electronica - Asamblata - 1200X600X800 Mm
NSYSF12680E Declaratie RoHS UE
Romanian
2024-04-24
NSYSF12680E Declaratie RoHS UE
Spacial Sf Carcasa Electronica - Asamblata - 1200X600X800 Mm
Fişa de instrucţiuni
Spacial SF (assembled supply) and main accessories - Instruction Sheet