This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
CAE
Spacial S3D CAE package for EPLAN
SILENT
2024-04-15
Declaratie de mediu
Spacial S3D - Steel Wall Mounting Enclosure
English
2024-04-15
Declaratie de conformitate
NSYTLCFL Declaratie REACh
Romanian
2024-04-03
NSYTLCFL Declaratie REACh
Standard Pentru Spacial S3D Dulap Ral7035, L245Xw130
NSYTLCFL Declaratie RoHS China
Romanian
2024-04-03
NSYTLCFL Declaratie RoHS China
Standard Pentru Spacial S3D Dulap Ral7035, L245Xw130
NSYTLCFL Declaratie RoHS UE
Romanian
2024-04-03
NSYTLCFL Declaratie RoHS UE
Standard Pentru Spacial S3D Dulap Ral7035, L245Xw130
CAD
Spacial SF - Cable-gland plates with FL type cut-out for cable-gland membranes - L245xW130 - 3D CAD