This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Declaratie de conformitate
NSYUTA22 Declaratie RoHS China
Romanian
2024-03-25
NSYUTA22 Declaratie RoHS China
Conectori UTA 20x20 pentru sina C simetrica, tip C20 si C40. Livrare, 20 buc.
NSYUTA22 Declaratie RoHS UE
Romanian
2024-03-25
NSYUTA22 Declaratie RoHS UE
Conectori UTA 20x20 pentru sina C simetrica, tip C20 si C40. Livrare, 20 buc.