In questo catalogo troverete tutti i componenti essenziali per realizzare quadri di comando di alta qualità. Scegliete i prodotti giusti per configurare le vostre apparecchiature con facilità, completare il vostro lavoro più velocemente e dare un impulso alla vostra attività.
PrismaSeT 6300 Catalog
English
2024-06-15
PrismaSeT 6300 Catalog
This catalog presents the Schneider Electric Low voltage switchboards PrismaSeT 6300.
This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
This new version of the document takes into account the launch of the new offers. It also takes into account the change in range name from all Spacial offer to PanelSeT and all Thalassa TBS/TBP to PanelSeT TBS/TBP.
In exposed environments, particular attention must be paid to the choice of enclosures. Stainless steel is the solution to resist aggression in exposed environments. This guide will help the reader to select the optimum stainless-steel enclosure accordingly.
Certificato
Test Certificato PrismaSeT P 3200A
Italian
2024-06-15
Test Certificato PrismaSeT P 4000A
Italian
2024-06-15
Dichiarazione di conformità
DECLARACION_DE_CONFORMIDAD_UE REJILLAS Y FILTROS CLIMASYS V-02-ES
Spanish
2024-05-30
DECLARATION DE CONFORMITÉ POUR GRILLES ET FILTRES CLIMASYS - FR