This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
This new version of the document takes into account the launch of the new offers. It also takes into account the change in range name from all Spacial offer to PanelSeT and all Thalassa TBS/TBP to PanelSeT TBS/TBP.
Certificato
Test certificato IEC 62208 Thalassa PLA - PHD
Italian
2024-06-15
Disclosure ambientale
PEP-Thalassa PLA
English
2024-06-15
Dichiarazione di conformità
NSYMUPLA124G Dichiarazione REACh
Italian
2024-06-13
NSYMUPLA124G Dichiarazione REACh
7035 Kit di affiancamento laterale 1200X400
NSYMUPLA124G Dichiarazione RoHS Cina
Italian
2024-06-13
NSYMUPLA124G Dichiarazione RoHS Cina
7035 Kit di affiancamento laterale 1200X400
NSYMUPLA124G Dichiarazione RoHS UE
Italian
2024-06-13
NSYMUPLA124G Dichiarazione RoHS UE
7035 Kit di affiancamento laterale 1200X400
Istruzioni
MOUNTING INSTRUCTIONS MUPLA
English,Spanish
2024-06-15
CAD
Thalassa PLA - Horizontal coupling kit for PLA enclosure H1250 - D420 mm - 3D CAD