This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Certificato
Test certificato IEC 62208 Thalassa PLA - PHD
Italian
2024-06-30
Disclosure ambientale
PEP-Thalassa PLA
English
2024-06-30
Dichiarazione di conformità
NSYMUPLA204G Dichiarazione REACh
Italian
2024-06-20
NSYMUPLA204G Dichiarazione REACh
7035 Kit di affiancamento laterale 2000x400
NSYMUPLA204G Dichiarazione RoHS Cina
Italian
2024-06-20
NSYMUPLA204G Dichiarazione RoHS Cina
7035 Kit di affiancamento laterale 2000x400
NSYMUPLA204G Dichiarazione RoHS UE
Italian
2024-06-20
NSYMUPLA204G Dichiarazione RoHS UE
7035 Kit di affiancamento laterale 2000x400
Istruzioni
MOUNTING INSTRUCTIONS MUPLA
English,Spanish
2024-06-30
CAD
Thalassa PLA - Horizontal coupling kit for PLA enclosure H2000 - D420 mm - 3D CAD