This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
This new version of the document takes into account the launch of the new offers. It also takes into account the change in range name from all Spacial offer to PanelSeT and all Thalassa TBS/TBP to PanelSeT TBS/TBP.
Disclosure ambientale
Spacial S3D - Steel Wall Mounting Enclosure
English
2024-07-15
Dichiarazione di conformità
NSYSD8R Dichiarazione REACh
Italian
2024-07-04
NSYSD8R Dichiarazione REACh
Pulpito con fondo asportabile L800 RAL7035
NSYSD8R Dichiarazione RoHS Cina
Italian
2024-07-04
NSYSD8R Dichiarazione RoHS Cina
Pulpito con fondo asportabile L800 RAL7035
NSYSD8R Dichiarazione RoHS UE
Italian
2024-07-04
NSYSD8R Dichiarazione RoHS UE
Pulpito con fondo asportabile L800 RAL7035
CAD
Spacial SD - Spacial SD H1000xW800xD597 A - 3D CAD