Use this document to:
- Install and operate your M241 Logic Controller.
- Connect the M241 Logic Controller to a programming device equipped with EcoStruxure Machine Expert software.
- Interface the M241 Logic Controller with I/O expansion modules, HMI, and other devices.
- Familiarize yourself with the M241 Logic Controller features.
This new firmware corrects several bugs, there is no functionality integrated. Details available in Release Notes.The firmware is delivered in 2 different shapes, for SD card or Seco package for SoMachine v4.3. According to your preferred way to update the firmware, you can select one shape or another.
M241 M251 Firmware
English
2024-07-15
M241 M251 Firmware
This new firmware correct an issue identified by the Err LED blinking and the PLC not booting.The firmware is delivered in 2 different shapes, for SD card or Seco package for SoMachine v4.3. According to your preferred way to update the firmware, you can select one shape or another.
New firmware for M241 v4.0.6.41
English
2024-07-15
New firmware for M241 v4.0.6.41
This new firmware updates the memory driver to integrate new component references, and corrects several anomalies, with details in the Release Notes.
New firmware for M241 v4.0.6.42
English
2024-07-15
New firmware for M241 v4.0.6.42
This new firmware address the anomaly of M241 firmware update with V5.0.8.4, with LED Error blinking.
Dichiarazione di conformità
TM241CEC24T Dichiarazione REACh
Italian
2024-07-15
TM241CEC24T Dichiarazione REACh
Controllore M241 24 I/O transistor PNP, Ethernet, CAN master
TM241CEC24T Dichiarazione RoHS UE
Italian
2024-07-15
TM241CEC24T Dichiarazione RoHS UE
Controllore M241 24 I/O transistor PNP, Ethernet, CAN master
Compact Hardwired Logic Controller M241, System User Guide
English
2024-07-15
Compact Hardwired Logic Controller M241, System User Guide
This document describes a generic architecture based on Modicon M241 Logic Controller and is intended to provide a quick introduction to the described system.