"This document addresses the firmware compatibility, exceptions, and recommendations for Modicon modules"
Modicon M580 Complex Topologies, System Guide
English
2024-04-15
Modicon M580 Complex Topologies, System Guide
This document presents one of the EcoStruxure™ Plant features, using Ethernet as thebackbone around the Modicon M580 offer to facilitate communications between an M580local rack and remote sub-rings through dual-ring switches (DRSs).
Quantum EIO - Remote I/O Modules, Installation and Configuration Guide
English
2024-04-15
Quantum EIO - Remote I/O Modules, Installation and Configuration Guide
This guide describes these modules and their roles in a Quantum EIO system:- 140 CRP 312 00: remote I/O head module on a Quantum local rack in a remote I/O main ring- 140 CRA 312 00: remote I/O adapter module in a Quantum remote I/O drop- BMX CRA 312 .0: remote I/O adapter module in a Modicon X80Modicon X80 remote I/O drop
Quantum EIO, System Planning Guide
English
2024-04-15
Quantum EIO, System Planning Guide
This guide provides detailed information about the Quantum EIO system, including the following:
- Ethernet remote I/O networks
- topology rules and recommendations for choosing a network configuration
- role of DRSs
- system commissioning and maintenance
- system performance and limitations
- system diagnostics
CLASS - C225351 - PROGRAMMABLE CONTROLLER,CLASS - C225802 - PROCESS CONTROL EQUIPMENT-For Hazardous Locations
Modicon Quantum, Certificate, IACS, LR, Marine
English
2024-04-15
Modicon, Certificate, UL, Ordinary Location
English
2024-04-15
Modicon, Certificate, UL, Ordinary Location
UL certificate for USA and Canada
Firmware
M580 BMxCRA312x0 Operating System
English
2024-04-15
M580 BMxCRA312x0 Operating System
Refer to "??.pdf" for further details.Our firmware is continuously reviewed and updated in order to maintain the highest level of quality of our products. Schneider Electric recommends to all customers to ensure that their installation is up to date with the newest firmware versions, to protect their infrastructures against cybersecurity threats and experience the best quality. For further information please visit the Schneider Electric Cybersecurity Support Portal: https://www.se.com/ww/en/work/support/cybersecurity/overview.jsp
Declaration of Conformity
140CRA31200 RoHS-deklaration för EU
Swedish
2024-04-19
140CRA31200 RoHS-deklaration för EU
ERIO-drop modul, 2+1 TX
140CRA31200 RoHS-deklaration för Kina
Swedish
2024-04-19
140CRA31200 RoHS-deklaration för Kina
ERIO-drop modul, 2+1 TX
Katalog
Discover catalog for Modicon Quantum automation platform
English
2024-04-15
Declaration of Conformity
ACMA_RCM_QUANTUM_AUG2017
English,French
2024-04-15
ACMA_RCM_QUANTUM_AUG2017
Australian Communications and Media Authority (ACMA)
The Quantum 140CRA31200 module is the adapter module used to connect a Quantum drop in a Quantum or an M580 EIO installation. The Quantum 140CRA31908 module is the adapter module needed to connect an S908 bus in an M580 EIO installation.