This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
This new version of the document takes into account the launch of the new offers. It also takes into account the change in range name from all Spacial offer to PanelSeT and all Thalassa TBS/TBP to PanelSeT TBS/TBP.
CAE
Spacial CRN CAE package for EPLAN
SILENT
2024-06-20
Spacial S3D CAE package for EPLAN
SILENT
2024-06-19
Spacial SM CAE package for EPLAN
SILENT
2024-06-19
Miljöinformation
UE_Spacial SF, Steel floor-standing enclosure
English
2024-06-15
Declaration of Conformity
NSYDPA44 REACh-deklaration
Swedish
2024-06-26
NSYDPA44 REACh-deklaration
Ritningsficka i plast för A4 . Mått (hxbxd) 234x278x40 mm Färg RAL7035
NSYDPA44 RoHS-deklaration för EU
Swedish
2024-06-26
NSYDPA44 RoHS-deklaration för EU
Ritningsficka i plast för A4 . Mått (hxbxd) 234x278x40 mm Färg RAL7035
NSYDPA44 RoHS-deklaration för Kina
Swedish
2024-06-26
NSYDPA44 RoHS-deklaration för Kina
Ritningsficka i plast för A4 . Mått (hxbxd) 234x278x40 mm Färg RAL7035