This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
This new version of the document takes into account the launch of the new offers. It also takes into account the change in range name from all Spacial offer to PanelSeT and all Thalassa TBS/TBP to PanelSeT TBS/TBP.
Universal Enclosures - Quick Selection Guide without CRN (2024 EN)
English
2024-06-19
Universal Enclosures - Quick Selection Guide without CRN (2024 EN)
This new version of the document takes into account the launch of the new offers. It also takes into account the change in range name from all Spacial offer to PanelSeT and all Thalassa TBS/TBP to PanelSeT TBS/TBP.
In exposed environments, particular attention must be paid to the choice of enclosures. Stainless steel is the solution to resist aggression in exposed environments. This guide will help the reader to select the optimum stainless-steel enclosure accordingly.
CAE
Spacial S3D CAE package for EPLAN
SILENT
2024-06-19
Declaratie de mediu
Spacial S3D - Steel Wall Mounting Enclosure
English
2024-06-19
Declaratie de conformitate
NSYPIN75 Declaratie REACh
Romanian
2024-06-21
NSYPIN75 Declaratie REACh
Usa interioara pentru Spacial WM din otel H700xW500, RAL7035, ajustabila in adancime
NSYPIN75 Declaratie RoHS China
Romanian
2024-06-21
NSYPIN75 Declaratie RoHS China
Usa interioara pentru Spacial WM din otel H700xW500, RAL7035, ajustabila in adancime
NSYPIN75 Declaratie RoHS UE
Romanian
2024-06-21
NSYPIN75 Declaratie RoHS UE
Usa interioara pentru Spacial WM din otel H700xW500, RAL7035, ajustabila in adancime
Ghidul utilizatorului
User manual for Spacial CRN(G) INNER DOOR
SILENT
2024-06-20
Software lansat
Ghid de alegere CaSys
English
2024-06-15
CAD
Spacial S3D CRN S3X - H700xW500 - Internal door - 3D CAD