This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
Openbaarmaking milieugegevens
Spacial S3D - Steel Wall Mounting Enclosure
English
2024-04-15
Conformiteitsverklaring
NSYTHL1242EPLM China RoHS-verklaring
Dutch
2024-04-16
NSYTHL1242EPLM China RoHS-verklaring
Thalassa PLM - Handgreep met 1242E cilinderslot & sleutel
NSYTHL1242EPLM EU RoHS-verklaring
Dutch
2024-04-16
NSYTHL1242EPLM EU RoHS-verklaring
Thalassa PLM - Handgreep met 1242E cilinderslot & sleutel
NSYTHL1242EPLM REACh-verklaring
Dutch
2024-04-16
NSYTHL1242EPLM REACh-verklaring
Thalassa PLM - Handgreep met 1242E cilinderslot & sleutel
Instructieleaflet
Thalassa PLM General Instruction for external handle with barrel & key
SILENT
2024-04-15
CAD
Thalassa PLM - Handle with 1242E barrel and key - 3D CAD