This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Conformiteitsverklaring
DoC
Russian
2024-04-15
Instructieleaflet
PrismaSeT P IP30/IP55 enclosure - Instruction Sheet