This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Openbaarmaking milieugegevens
UE_Spacial SF, Steel floor-standing enclosure
English
2024-04-15
Conformiteitsverklaring
NSYCW33 China RoHS-verklaring
Dutch
2024-04-24
NSYCW33 China RoHS-verklaring
"Spacial - Controlevenster - IP55 - 300x300mm"
NSYCW33 EU RoHS-verklaring
Dutch
2024-04-24
NSYCW33 EU RoHS-verklaring
"Spacial - Controlevenster - IP55 - 300x300mm"
NSYCW33 REACh-verklaring
Dutch
2024-04-24
NSYCW33 REACh-verklaring
"Spacial - Controlevenster - IP55 - 300x300mm"
Instructieleaflet
Instruction Sheet - NSYCW Control window with aluminum frame and acrylic window