This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
Conformiteitsverklaring
NSYCW55 China RoHS-verklaring
Dutch
2024-03-29
NSYCW55 China RoHS-verklaring
"Spacial - Controlevenster - IP55 - 500x500mm"
NSYCW55 EU RoHS-verklaring
Dutch
2024-03-29
NSYCW55 EU RoHS-verklaring
"Spacial - Controlevenster - IP55 - 500x500mm"
NSYCW55 REACh-verklaring
Dutch
2024-03-29
NSYCW55 REACh-verklaring
"Spacial - Controlevenster - IP55 - 500x500mm"
Openbaarmaking milieugegevens
Spacial S3D - Steel Wall Mounting Enclosure
English
2024-04-15
Instructieleaflet
Instruction Sheet - NSYCW Control window with aluminum frame and acrylic window