Short-Circuit Current Ratings (SCCR) and branch circuit protection
The table shows recommended fuse ratings for UL and CSA requirements.
The components are for use together in accordance with standard UL508
2_ATV312 Installation Manual
English
2024-04-15
3) ATV312 programming manual
English
2024-04-15
3) ATV312 programming manual
V5.1IE57
ATV312 CANopen manual
English
2024-04-15
ATV312 DeviceNet manual
English
2024-04-15
ATV312 PROFIBUS DP communication manual
English
2024-04-15
ATV312 to ATV320 Migration Manual
English
2024-04-15
Instruction sheet
Instruction Sheet: China RoHS - Hazardous Substances Table
Chinese,English
2024-04-15
Instruction Sheet: China RoHS - Hazardous Substances Table
This table is made according to SJ/T 11364. O: indicates that the concentration of a hazardous substance in all of the homogeneous materials for this part is below the limit as stipulated in GB/T 26572. X: indicates that the concentration of a hazardous substance in at least one of the homogeneous materials used for this part is above the limit as stipulated in GB/T 26572
Catalogue
Discover catalogue for Altivar 312 variable speed drives