This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
Environmental disclosure
UE_Spacial SF, Steel floor-standing enclosure
English
2024-05-15
CAE
Spacial SM CAE package for EPLAN
SILENT
2024-05-15
Declaration of conformity
NSYMFB China RoHS Declaration
English
2024-05-14
NSYMFB China RoHS Declaration
Fixing brackets for internal fixing of vertical rails at the same level of base
NSYMFB EU RoHS Declaration
English
2024-05-14
NSYMFB EU RoHS Declaration
Fixing brackets for internal fixing of vertical rails at the same level of base
NSYMFB REACh Declaration
English
2024-05-14
NSYMFB REACh Declaration
Fixing brackets for internal fixing of vertical rails at the same level of base
Instruction sheet
Instruction Sheet for internal fixing bracket of vertical rails - same level of base