This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU. Taking into account the change in range name going from Spacial SF to PanelSeT SFN. This version as well provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view of the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased-out references
"This new version of the document takes into account the launch of 2 new offers, PanelSeT SFN and Climasys CU, with a change in range name going from Spacial SF to PanelSeT SFN. This version as well, provides a view on the merge between CRN and CRNG offers into one single one. It also gives a view on the new Customization services tool. It also takes into account some changes to the ranges, with the suppression of phased references"
Environmental disclosure
UE_Spacial SF, Steel floor-standing enclosure
English
2024-04-15
Declaration of conformity
NSYSIBTB China RoHS Declaration
English
2024-04-03
NSYSIBTB China RoHS Declaration
Spacial SF brackets for fixing intermediate mounting plates back to back
NSYSIBTB EU RoHS Declaration
English
2024-04-03
NSYSIBTB EU RoHS Declaration
Spacial SF brackets for fixing intermediate mounting plates back to back
NSYSIBTB REACh Declaration
English
2024-04-03
NSYSIBTB REACh Declaration
Spacial SF brackets for fixing intermediate mounting plates back to back
Instruction sheet
Post-fixing device for Spacial wall-mounting enclosure
SILENT
2024-04-15
CAD
2 Back Fixing Inter. Chassis
SILENT
2024-03-13
Spacial SM-SF - Brackets for fixing mounting plates in back-to-back position - 3D CAD